By Language / English
Steam Systems III: Distribution, Control & Regulation of Steam
Steam is one of the oldest and most widely used forms of energy in industry. Difficulties in energy
management of steam arise from the fact that it is often a totally unmeasured service. The
distribution, control and regulation of steam is crucial because inefficiency translates into
additional operating costs. The savings potential is enormous: Not only from a fiscal standpoint,
but also from an environmental standpoint. This course will review the basics of steam systems
and list the benefits associated with measuring steam. We will discuss steam piping design,
metering, and steam manifolds. Also addressed are two typical applications of tracing as well as
the components involved when controlling and regulating steam.
Topic :
Boilers and steam systems